How to use Selected Optimized Coordination user interface
Dowload a quick start help in pdf!
Protection Device
It is possible to select/deselect more than one type of short circuit protection device by clicking directly on the items. When a device has been selected, the field turns grey.
If you hold the mouse over the selectable items, helpful popup texts will appear.
Rated Voltage
It is possible to select/deselect more than one voltage by clicking directly on the voltage
When a voltage has been selected, the field turns grey.
Short Circuit Current
It is possible to select/deselect more than one short circuit current level by clicking directly on the currents. Selected fields turn grey.
Starter Type
It is possible to select/deselect one or more starter types by clicking on the types.
If you hold the mouse over the selectable items, helpful popup texts will be displayed.
Coordination Type
It is possible to select/deselect one or more coordination types by clicking on the types.
If you hold the mouse over the selectable items, helpful popup texts will appear.
Rated Motor Power
It is possible to select/deselect one or more rated motor powers by clicking on the kW sizes. "Overview" is the default choice: the first available motor power for every coordination table is shown. You can than press the “>>” symbol to get the whole coordination table, with all the available motor powers.
Selected fields turn grey.
Clear selections
When you press “clear selections”, all selected values will be deselected.
Results
When you have selected the values, which are most appropriate to your application, only a limited number of solutions will be displayed. The number of search results will be displayed at the bottom of the page. In the right side corner it is possible to select how many results you want to have displayed.
The “Enable Smart Current Search” is a feature for the short circuit current where “near to” selected values also are included in the result.
To see the results, scroll down on the page, press the “>>” symbol on the right hand side of the page. The page will load the selected table. It is now possible to print the page to a pdf file or print the page, by pressing the Export To Pdf | Print texts placed just above the left hand side of the table.
To go back to the selection, press Back in the left hand side above the table or use normal browser functions.
To see the results previously selected, scroll down on the page.